Metal Working Factory

Galvanized Steel vs Aluminum: Key Comparisons

Author: Scott Bredemann

Updated: 08/22/2024 | Read Time: 5 mins

When choosing between galvanized steel and aluminum, understanding their unique properties is essential for selecting the right material for your project. Both materials are widely used in industries such as construction, manufacturing, and automotive, but they serve different purposes depending on factors like strength, weight, and corrosion resistance.

Galvanized steel is known for its durability and cost-effectiveness, making it a popular choice for structural applications. On the other hand, aluminum is lightweight, resistant to corrosion, and ideal for environments where weight savings are crucial.

In this article, we’ll compare galvanized steel and aluminum, exploring their strengths, weaknesses, and best use cases to help you make an informed decision.

What is Galvanized Steel?

Galvanized steel is a type of steel that has been coated with a protective layer of zinc to prevent rust and corrosion. This galvanization process enhances the metal’s durability, making it a popular choice for outdoor and heavy-duty applications. The zinc coating acts as a barrier against moisture and oxidation, extending the lifespan of the steel even in harsh environments.

Common uses for galvanized steel include construction materials (beams, roofing, fencing), automotive parts, and industrial equipment. It is valued for its strength, affordability, and resistance to wear and tear, though it tends to be heavier than aluminum and may not be as flexible for certain applications.

What is Aluminum?

Aluminum is a lightweight, corrosion-resistant metal known for its versatility and durability. Unlike steel, aluminum naturally forms a protective oxide layer that prevents rust, making it ideal for moisture-prone environments. It is also highly malleable, allowing for easy shaping, machining, and fabrication.

Common applications include aerospace, automotive, electronics, and construction. While aluminum is not as strong as galvanized steel, its high strength-to-weight ratio makes it a preferred choice for projects where reducing weight is critical. Additionally, aluminum’s non-magnetic and conductive properties make it valuable in electrical and heat transfer applications.

Aluminum and Galvanized Steel Warehouse

Physical Property Comparisons

PropertyGalvanized SteelAluminum
Density~7.85 g/cm³~2.7 g/cm³ (about 1/3 the weight of steel)
StrengthHigher tensile strength (~250-550 MPa)Lower tensile strength (~90-300 MPa)
Corrosion ResistanceGood (due to zinc coating) but can degrade over timeExcellent (forms natural oxide layer)
WeightHeavierLightweight (about 1/3 the weight of steel)
DurabilityVery durable but can rust if coating is damagedLess durable but resistant to rust
MachinabilityHarder to machine, requires special toolsEasier to machine and fabricate
Electrical ConductivityLow conductivityHigh conductivity (about 60% of copper’s conductivity)
Thermal ConductivityLower than aluminum (~45-60 W/m·K)High (~200-235 W/m·K)
FlexibilityLess flexible, more rigidMore malleable and easier to shape
CostGenerally lower than aluminumMore expensive than galvanized steel
Galvanized Steel vs. Aluminum Physical Properties Table

Chemical Property Comparisons

PropertyGalvanized SteelAluminum
CompositionSteel (iron + carbon) with a zinc coatingPrimarily aluminum (often alloyed with other metals)
Corrosion ResistanceRelies on zinc coating; can corrode if damaged or exposed to harsh chemicalsForms a natural oxide layer that resists corrosion
Oxidation ReactionZinc coating slows oxidation, but once it wears off, steel rustsForms aluminum oxide, which protects against further oxidation
ReactivityIron in steel is highly reactive when exposed to moisture and oxygenLess reactive due to strong oxide layer formation
Galvanic CorrosionCan corrode rapidly when in contact with aluminum or copper in wet environmentsCan corrode when in contact with steel due to galvanic reaction
Acid ResistanceZinc coating dissolves in strong acidsModerate resistance but can corrode in strong acids or bases
Base ResistanceZinc coating offers some resistance, but steel can be affectedCan react with strong alkaline solutions
Melting Point~1,370°C (2,500°F) (steel core); Zinc melts at ~420°C (788°F)~660°C (1,220°F)
Galvanized Steel vs. Aluminum Chemical Properties Table

Choosing the Right Metal for Your Application

When deciding between galvanized steel and aluminum, the best choice depends on the specific requirements of your application. Here are key factors to consider:

  • Strength and Load-Bearing Needs – If your project requires a high-strength material for structural support, galvanized steel is the better option due to its superior tensile strength and durability. It’s commonly used in construction, heavy machinery, and industrial frameworks.
  • Weight Considerations – If minimizing weight is a priority, aluminum is the ideal choice. It’s about one-third the weight of steel, making it perfect for transportation, aerospace, and lightweight structural applications where reducing mass improves efficiency.
  • Corrosion Resistance – For environments exposed to moisture, chemicals, or extreme weather, aluminum has an advantage because of its natural oxidation layer that resists rust. Galvanized steel also resists corrosion but may degrade over time if the zinc coating wears off.
  • Fabrication and Machining – If your project requires easy shaping, welding, or machining, aluminum is generally more malleable and easier to work with compared to galvanized steel, which is harder and requires special tools for processing.
  • Cost and Budget – Galvanized steel is typically more affordable than aluminum, making it a better choice for budget-conscious projects. However, aluminum’s longevity in corrosive environments can offset its higher initial cost through reduced maintenance and longer lifespan.

By assessing your project’s strength, weight, corrosion resistance, and cost requirements, you can determine whether galvanized steel or aluminum is the better material for your application.

Metal Gears and Cogs

Industry-Specific Considerations

Different industries have unique requirements when choosing between galvanized steel and aluminum:

  • Construction – Galvanized steel is preferred for structural applications like beams, roofing, and fencing due to its high strength. Aluminum is used in decorative elements and lightweight structures.
  • Automotive & Transportation – Aluminum is widely used in vehicles and aerospace applications to reduce weight and improve fuel efficiency, while galvanized steel is used in heavy-duty truck frames and infrastructure.
  • Manufacturing & Industrial Components – Galvanized steel is ideal for heavy-duty machinery and industrial frameworks, whereas aluminum is used in precision parts and electrical enclosures due to its conductivity and corrosion resistance.

Selecting the right material depends on the industry’s specific demands for strength, weight, durability, and corrosion resistance.

Parting Thoughts

We hope this article has provided valuable insights into the differences between galvanized steel and aluminum in industrial manufacturing. If you’re interested in learning more about other essential metals, be sure to check out our articles on aluminum alloys, copper, lead, and more. Looking for high-quality galvanized steel or aluminum components? 

Explore our extensive catalog, including: aluminum extrusions, and precision components. Need something customized? Visit our Rapid Design page to configure parts to your exact specifications.Have questions? Contact our product experts for guidance in selecting the best materials for your application. Get the precision, flexibility, and reliability you need—only at MISUMI USA.