Updated: October 15, 2024
As the holiday season approaches, it’s amazing how many moments you have of nostalgia regarding events in your life. Personally, one such event was the gift of a Nintendo™ gaming system. I can easily remember the excitement myself and my friends had when we played this console. We found ourselves amazed by what it did, not realizing that the investment in all the games will come at a cost one day as even more advanced consoles will come into existence.

Jump ahead 4-5 years and something even more unexpected happened: the release of multiple gaming consoles. Not only did you have the upgrade to the Nintendo™ in form of the Super Nintendo™ but also the release of the Sega™ Genesis a year prior. As any owner of the Nintendo™ knew, there were two things that were dreaded, one being no backward compatibility and the other, no cross-platform play. This was not a happy thought, but it was what it was.
Fast forward another 5 years to the launch of Sony’s Playstation™ (PS1) and the advancement from hard cartridges to that of compact discs. Not only could you play games but also music CD’s. Another big advancement came when the Playstation 2™ (PS2) was launched. Since the first and second systems used the same size disc, you could play the older games on the newer system. This meant that your game library did not immediately become obsolete. Your investment in the platform was not wiped out.
These actions and concepts are dreaded and transcend more than just the gaming industry. Network connectivity can produce similar concerns. For example, if you are running an older PLC with a Cat5 Ethernet port, where can you find a replacement cable?
A quick search pulls up plenty of Cat5e and Cat6 options, but will this be just like some gaming consoles and not work with the older system? Does the presence of new Ethernet cable features like shielding affect compatibility? Yeah! And what’s with all this Cat7 talk already?
Fortunately, the technology in this field is designed with backward compatibility and thus will work with older equipment. So, if you do have a Cat5 input, you can use any generation of cable developed after it. In this case, you can use the readily available and inexpensive Cat5e cables.
If those are out of stock or you want to transmit more data then Cat6 or Cat6a cables are available. Should you want to move to where the industry is headed, then some Cat7 options are available, and feel free to choose that cable instead. If you’re concerned about the presence of shielding because your old cable did have it, fear not because it will work too.
If the age of your hardware and whether you can find replacement components are concerns, you can sleep soundly. Most Cat5, Cat6/6a, and Cat7 products are designed to work backwards with older technology.
MISUMI has access to all your Cat5e, Cat6/6a, and Cat7 needs. If you’re considering a new gaming system, rest assured you will very likely be able to play all the older ones you’ve collected as well.