How to Build Smarter Machines: An Overview of Frames, Drives, Guides, and Controls

Published on
November 4, 2025

12 min read

From compact robotic cells to fully integrated production lines, we’re entering a new era of automation. This requires uncovering ways to build smarter, faster, and more flexible and reliable systems that can adapt easily to changes.

To prepare, let’s start at the beginning. This article highlights basic foundational machine design elements: frames, guides, drives, and controls.  

1. Designing Frames 

frames, an aluminum extrusion software

There are different types of frame materials. Some of the most common materials include sheet metal, welded frames, wood, and aluminum extrusions.

Aluminum extrusions are a common choice for machine design since they are lightweight, cost-effective, corrosion resistant, and provide flexibility. Not to mention, they are also aesthetically-pleasing.

Here are few things to consider if you’re leaning towards aluminum for your frame design.

  • Aluminum is weaker than steel.
  • Aluminum uses bolt and screw type of connections, which are not as permanent as welding.
  • Extrusions are not as rigid compared to other common types like steel, but there are extrusion types that offer higher rigidity.

You also want to consider scalability. Whether you’re planning to increase throughput, integrate new automation technology, or add vision inspection, the frame should accommodate these updates without requiring a total redesign. Using standardized, configurable frame elements (with precise cut lengths and machining options available on demand) makes scaling up or retooling a straightforward process.  

Common Extrusion Types

Aluminum extrusions come in a wide variety of shapes and sizes, as well as anodizing options, with the most common being a standard square shape.

Here is a quick comparison of aluminum extrusions types:

Aluminum Extrusion TypesKey CharacteristicsBest For / Typical ApplicationMISUMI Product Example (By Part Number)
Standard Aluminum ExtrusionBalanced strength and weight; versatile slot configurationsGeneral automation frames, enclosures, workstationsHFS5-2020
High-Rigidity ExtrusionThicker walls and reinforced cross-sections for high load capacityMachine bases, gantry systems, heavy-duty automationGFS8-4040
Lightweight ExtrusionReduced wall thickness for lower mass while maintaining accuracyPortable systems, adjustable guards, test setupsHFSL6-3030
Bend Slot / Parallel Chamfer TypeCurved or multi-axis profiles with aligned or flexible slot orientations; allow creative or ergonomic frame layoutsRounded guarding, ergonomic cells, and modular equipment needing flexible mountingHFSP5-2020
Mixed Slot / Small Corners TypeCombines varied slot orientations with compact geometry for space efficiency and flexible mountingReconfigurable workcells, compact equipment, and tight-space automation framesHFSV6-3030

There are also different types of coating options:

Surface TreatmentKey CharacteristicsBest For / Typical Application
Clear AnodizedStandard corrosion resistance; professional appearanceCleanroom, lab automation, general environments
Black AnodizedLow reflectivity and high surface hardnessVision inspection systems, optical setups, premium equipment
Yellow (Baked-On Finish) Visual safety indication, easy identification of guarded areasMachine guarding, operator-accessible zones

Design Faster with FRAMES

FRAMES, an aluminum extrusion design software, makes the design or reconfiguration process easy with drag-and-drop capabilities and joints and brackets automatically added as you design. You can download the free software here.

Aluminum Extrusion Accessories

The basic assembly of a frame is simple: the extrusion, bracket, and nuts and bolts.

But there are several accessories you can use to elevate your frame design, such as:

2. Choosing the Right Guide

 

The right guides will achieve smooth, accurate motion that your design requires. Components like linear bearings, shafts, rails, and bushings ensure other parts move along a defined path with little friction.  

For high-precision applications, even a fraction of a millimeter of misalignment can cascade into product defects or premature wear.  

Here are some things to consider when choosing a guide system: 

  • Maintains parallelism and straightness across long travel distances.
  • Minimizes vibration, backlash, and drift.
  • Reduces maintenance needs and extends component life. 
  • Supports heavier loads without compromising accuracy. 

The right guide depends on the application’s load, speed, environment, and accuracy requirements. Let’s take a look at the most common guides found in industrial automation applications.

Guide TypeUse CaseCommon Applications
Linear Ball Bearings
misumi short linear ball bearing
Linear ball bearings support the load of a carriage during single-axis movement and provide a low friction. Linear shafts for linear ball bearings are available in different lengths, materials, and tolerances. CNC machines, 3D printers, imaging and surgical robots, and packaging and printing equipment.
Bushings
misumi straight linear plain bushing
Bushings help to reduce friction during motion and constrain motion to one axis. They help to move parts smoothly and easily. They are used in a wide of range of applications that have a light/moderate load and require low accuracy. They are also low in cost.Fitness equipment, packaging machinery, 3D printers, and assembly jigs.
Linear Guides
misumi linear guide assembly
Linear guides are a bearing that uses recirculating balls or rollers to reduce friction and constrain motion to one axis or one direction. They are ideal for applications that require moving parts smoothly and easily when they have moderate/high loads and are high rigidity. CNC machines, microscopes, water jets, X-ray machines, robot transfer units, automotive assembly fixtures, 3D printers, and packaging machines.
Cam Followers
misumi cam followers
Cam followers minimize friction via rolling motion, making them ideal for supporting loads or guiding motion along a defined path.Packaging machines, medical equipment, pick and place machines, clamps and grippers, and bottling machines.
Rotary Bearings
misumi rotary bearing
Ball and roller bearings consist of hardened steel rolling elements positioned between an inner and outer race, enabling high-speed, low-friction rotation. Proper implementation improves machine efficiency and minimizes noise and heat. Automotive, robotics,. production machines, conveyors, and medical equipment.
Rollers
conveyor rollers misumi
Conveyor rollers are used in conveyor systems to facilitate the movement of goods and materials. They are designed to reduce friction and provide smooth transportation, making them essential components in manufacturing and logistics. Assembly lines, workstations, warehousing, and packaging lines.
Spline Shafts
misumi ball splines
Spline shafts have ridges or teeth that mesh with grooves in a mating part, such as a gear or hub, to transmit torque while maintaining alignment. Paper manufacturing, robotic arms, pick-and-place machines, CNC machines, and automated packaging equipment.
Rod End Bearings
misumi rod end bearings
Rod end bearings allow for rotational movement between different parts. They consist of a spherical outer surface that fits into a housing, providing a pivot point. Robotics, material handling and equipment, positioning systems, and packaging machines.

MISUMI offers a variety of linear guides along with several grease options (high temp, clean room, and self lubricating). With MISUMI, you can specify stroke length, preload, surface treatment, and material to get the right part needed, rather than going fully custom.

Integrating Guides with the Frame 

When integrating guides with the frame, here are some tips:  

  • Design rigid mounting points and minimize joint interfaces.
  • Use machined reference surfaces or locating features in your frame.
  • Ensure thermal and mechanical loads are evenly distributed across the guide. 

3. Driving Efficiency with Smart Actuation 

Whether electric, pneumatic, hydraulic, or manual — drives convert power into controlled, repeatable motion. Selecting the right actuation solution can boost efficiency, reduce energy consumption, and extend machine life. 

On the other hand, the wrong drive can cause vibration, heat buildup, excessive wear, and even premature failure.  

Common Drive Methods

Here is an overview of some of the different drive methods, including product examples:

Drive TypeUse CaseCommon Applications
Ball Screws
misumi ball screw
Ball screws converts rotary motion to linear motion, offers precision movement for various applications, and are designed to minimize friction and wear.CNC machines, X-ray machines, DNA sequences, 3D printers, packaging machines, airplanes, and car power steering.
Timing Belts & Pulleys
misumi timing belt
Timing belts transmit torque to other components or convert rotary motion into linear motion. They are low cost and suitable for a wide range of loads and accuracy requirements.Fitness equipment, packaging machinery, 3D printers, conveyors, low-cost CNC machines, and medical lab automation.
Chain & Sprockets
chain and sprockets
Chains are used to transmit torque generated by a power source to other machinery or parts and are usually used in combination with geared machinery called sprockets.Power transmission, material handling systems, automotive, assembly lines, and packaging equipment.
Gears
misumi gear
Gears are offered in a variety of types, including spur, helical, bevel, worm, and rack and pinion. They are often categorized by their shaft orientation (parallel, intersecting, or non-parallel and non-intersecting), tooth type (straight, angled, or curved), or function.Conveyor systems, robotics, medical equipment, assembly lines, material handling, aerospace, and automotive.
Hydraulic Cylinders
SMC hydraulic cylinder
Hydraulic cylinders convert fluid into linear motion and are used to push, pull, lift, or press. Hydraulic presses, material handling, and aerospace.
Air/Pneumatic Cylinders
smc air cylinder
Air cylinders convert compressed air into linear motion by using air pressure to move a piston inside a barrel, which then moves a connected rod that can be used to clamp, lift or push. Assembly lines, packaging, sorting and handling, aerospace, medical, and automotive.
Motorized Rotary Stages
misumi motorized rotary image
Motorized rotary stages are precision devices that enable rotational movement in a controlled and automated manner. These stages provide accurate positioning and smooth rotation, making them vital for tasks that require precise alignment and orientation. Robotics, microscopy, and optical measurement.
Manual Drives
Elesa-Bridge-Handle-Antimicrobial-Protection-EBP-Series
Manual drives can be designed using handles, wheels, and/or levers, such as door and drawer handles.Storage solutions, medical and lab equipment, electronic enclosures, motion controls, material handling, and safety mechanisms.

Integrating Drives with Guides and Frames 

Proper integration between the drive system, guides, and frame is essential. Here are some tips:

  • Mount motors and actuators directly to rigid, vibration-resistant surfaces. 
  • Align actuators with guides to prevent side loads that increase wear.
  • Use modular drive mounts to simplify maintenance and future upgrades. 

4. Choosing Controls that Integrate and Offer Scalability 

Controls connect mechanics and intelligence and dictates how smoothly your machine moves, responds to feedback, and adapts to changing conditions. For best performance, select controls that integrate seamlessly with your drives and mechanical systems, match the precision requirements of your application, and provide flexibility for future upgrades. 

controls systems overview

Even the most sophisticated controller is ineffective if it cannot communicate with your drives, sensors, and actuators. Proper integration ensures: 

  • Reliable and repeatable motion. 
  • Simplified commissioning and reduced debugging time. 
  • Lower risk of errors during maintenance or upgrades. 

Most automated machinery or systems nowadays have some sort of electrical interface that allows the operator to interact with the operation and control of the machine. Human-Machine Interfaces (HMIs) and Programable Logic Controllers (PLCs) are two key components that can be used individually but are often used together to operate and monitor machinery and processes.

Overview of PLC

A PLC is a specialized computer system used for industrial automation, controlling machines and entire production lines by receiving inputs, applying programmed logic, and driving outputs.

It operates without conventional computer peripherals (like display or keyboard) and serves to integrate mechanical and electrical systems seamlessly.

PLCs come in a variety of sizes and with different capabilities, but they all include the following five components:

PLC ComponentDescriptionProduct Example
Central Processing Unit (CPU)The “brain” of the PLC where software logic resides; it processes inputs and determines outputs. Mitsubishi-Electric-Automation-MELSEC-iQ-F-FX5U-Series-Sequencer-CPU
Mitsubishi Electric Automation MELSEC iQ-F FX5U Series Sequencer CPU
Input ModuleInterfaces with field sensors (digital or analog) to capture signals from the outside world. Mitsubishi-Electric-Automation-MELSEC-Q-Series-Input-Unit
Mitsubishi Electric Automation MELSEC-Q Series Input Unit
Output ModuleDrives downstream devices (motors, lights, drives etc.) based on CPU decisions.Mitsubishi-Electric-Automation-MELSEC-Q-Output-Unit
Mitsubishi Electric Automation MELSEC-Q Output Unit
Power SupplyConverts incoming line voltage (AC) to the required DC voltage (often 24 V) and often provides battery backup.MELSEC-Q-Series-Power-supply-unit
Mitsubishi Electric Automation MELSEC-Q Series Power Supply Unit
Programming Unit (HMI)

Allow operators to monitor/control processes, view KPIs, machine health etc. PLC-Touch-Panel-HMI-Display
Mitsubishi Electric Automation HMI Display, GOT2000 Series, GT27

To integrate a scalable PLC, start by understanding the specific application requirements and what tasks it will need to operate, your application’s environmental conditions, and ensure that the PLC you choose supports additional modules or functions.

Overview of HMIs

HMIs allow users to monitor relevant data and control the connected machines. Using programmable software, these devices can be configured to your specific needs.

While the term HMI can technically apply to any device that relays information to a human operator, most HMIs share several defining features including a screen, some form of input device, and programmable software.

It is important to keep in mind that HMIs are an extension of a PLC system, and that any data being processed by the PLC can be sent in some form directly to the HMI.

For example, say you wanted to implement an HMI for a robot that takes packages from a conveyor belt and places them onto pallets. You could program the HMI to display an overlay of the pallets, indicating how many packages are on each one. You could also add a camera feed from the robot arm POV to see what is being taken off the conveyor belt.

Machine design isn’t just about parts … 

… it’s about how parts work together.

Focus on integration, modularity, and adaptability, and you’ll succeed in building machines that perform better today and evolve seamlessly tomorrow. 

With the right combination of frames, guides, drives, and controls, you can turn complex machines into smart, efficient, and future-ready solutions.  

Struggling to find the right parts? MISUMI offers 80 sextillion part configurations and over 3,000 renowned mechanical and electrical brands. 

About the Author

Shannon Callarman

Shannon is an Associate Marketing Manager at MISUMI. She has over 10 years of experience partnering with manufacturers to help showcase their unique offerings and provide more value for engineers and OEMs. She has developed go-to-market and content strategies for a wide range of manufacturers, from industrial automation to silicone, to food packaging.

You may also like these